Export Sequencer List

Export and store a sequencer list from the AC Source application, then recall and run the stored sequencer at a later time.

  • By default, exported files are stored in the "Documents" folder on your computer and are organized by instrument type. For example, C:\Users\<user_name>\Documents\Keysight\PathWaveACSource\Sequencer\.
  • The default file name has a "SequenceList" prefix followed by the date and current time. For example, SequenceList 2021-11-20 11-40-26. To change the default name, click on the existing name and edit it.

See Also

Import Sequencer List